cancel
Showing results for 
Search instead for 
Did you mean: 

Clock configuration

arunease
Associate II
Posted on January 28, 2016 at 09:35

Hi, 

i am designing a board based on f329. The problem is,   i have a red mark on the clock configuration on HSI(16MHZ) and also 48MHZ clocks. when i am configuration with HSI(16MHZ). Could anyone tell me why ?

i have attached the screnshot. 
3 REPLIES 3
Nesrine M_O
Lead II
Posted on January 28, 2016 at 10:17

Hi emb_begin,

Could you please give us the right STM32 part number that you use, so we can help you?

You can set the clock value you need as target and CubeMX will do needed claculation for other parameters (M, N, P, Q).

-Syrine-

arunease
Associate II
Posted on January 28, 2016 at 11:21

its stm32439I.

 Do you have any example or configuration file for selecting HSI as clock source for PLL?
Amel NASRI
ST Employee
Posted on January 28, 2016 at 15:49

Hi emb_begin,

Please refer to

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00104712.pdf

and mainly the section ''Clock tree configuration view''. It describes how to use CubeMX for clock configuration.

CubeMX allows you to set a target frequency and it calculates other parameters based on this target and clock source.

-Mayla- 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.