2018-02-02 03:30 AM
I'm looking for a Clock configuration tool for STM32F429. Does one exist?
Or can I use the Clock configuration tool for STM32F40x/41x microcontrollers (AN3988)?
#stm32-f42018-02-02 03:52 AM
STM32CubeMX helps to configure clocking and generated RCC setup ( C code)
2018-02-02 04:46 AM
I'm going to use the STM32 Standard Peripheral Libraries (I like it more). I think the STM32CubeF4 is too bloated :-)
But I'm going to test the
STM32CubeMX at least to see if it generates what I need.
2018-02-02 05:59 AM
I would expect the earlier tool would work.
Top speed is now 180 MHz, with VCO in 192 to 432 MHz
The gearing here isn't unduly complicated, though the 180 MHz doesn't get you the 48 MHz used by USB internally, you'd need an external PHY to supply it's clock
I've built several 'fitter' tools, what clocks are you shooting for, from what HSE clock?
2018-02-05 05:32 AM
I tried the STM32CubeMx. But I notices in
SystemIni() that it is missing a call toSetSysClock(). Am I missing something?
void SystemInit(void)
{
/* FPU settings ------------------------------------------------------------*/
#if (__FPU_PRESENT == 1) && (__FPU_USED == 1)
SCB->CPACR |= ((3UL << 10*2)|(3UL << 11*2)); /* set CP10 and CP11 Full Access */
#endif
/* Reset the RCC clock configuration to the default reset state ------------*/
/* Set HSION bit */
RCC->CR |= (uint32_t)0x00000001;
/* Reset CFGR register */
RCC->CFGR = 0x00000000;
/* Reset HSEON, CSSON and PLLON bits */
RCC->CR &= (uint32_t)0xFEF6FFFF;
/* Reset PLLCFGR register */
RCC->PLLCFGR = 0x24003010;
/* Reset HSEBYP bit */
RCC->CR &= (uint32_t)0xFFFBFFFF;
/* Disable all interrupts */
RCC->CIR = 0x00000000;
#if defined (DATA_IN_ExtSRAM) || defined (DATA_IN_ExtSDRAM)
SystemInit_ExtMemCtl();
#endif /* DATA_IN_ExtSRAM || DATA_IN_ExtSDRAM */
/* Configure the Vector Table location add offset address ------------------*/
#ifdef VECT_TAB_SRAM
SCB->VTOR = SRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#else
SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2018-02-05 07:08 AM
CubeMX/HAL likely doing it in main() via SystemClock_Config(), although this is a bit late for external memories, etc.