2017-08-08 7:18 PM
Might as well learn something as long as the cubemx app isnt getting it right
I get stumped by the terminology sometimes because it tends to vary in the documentation.
In order to chain together two 16-bit timers into one 32 bit timer, I need to:
set up the first timer as oc output one pulse mode
do I want the slave in reset mode or gated mode?
2017-08-09 1:39 AM
First timer free running, with master output on update event (i.e. reset of the counter)
Second timer as slave External clock mode with proper ITRx input