cancel
Showing results for 
Search instead for 
Did you mean: 

Cant connect to stm32 discovery

shinobi
Associate
Posted on October 01, 2011 at 00:11

I have a problem with stm32 discovery. I am using IAR 6.21.3 and I constantly get the following error:

Fatal error: Faild to read CPUID from Cortex device

Session aborted!

ST-Link Utility is also giving me an error:

No target connected

Everything was running fine up until recently when I changed rcc (rcc_cfgr to be precise) and this error popped up. Since then I can't make any kind of connection with the board.

Please, give me some suggestions as to what could have gone wrong and how to fix it. Thanks in advance!
2 REPLIES 2
Posted on October 01, 2011 at 05:02

Get BOOT0 High (SB16 Off), and BOOT1 Low (SB2 On - Default), it will then boot into the system loader instead of your application.

Also be sure to use SWD mode.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
shinobi
Associate
Posted on October 01, 2011 at 19:18

It worked! Thank you so much!