2013-08-06 12:14 PM
I have begun programming the stm32f4. I made a really simple program first. It added one to r0 and stored the result in r0. Then I used
STM32 ST-LINK utility
to confirm that r0 is increasing. It was. I though I was on my way ... until now I made a program that still increments the registers, but I also setup timer8 for output compare to make a simple timer. The output pin I used does not change state. I usedSTM32 ST-LINK utility
to look at the memory contentes around the boundary address of timer 8 and found all the memory in that area is zeros. I tried to use the utility to change one of the timer 8 registers manually, and it told me ''error occurred during memory writing.'' The flash area of the memory displays correctly. Am I just unable to interact with the peripheral memory withSTM32 ST-LINK utility
? am I writing to the peripheral registers improperly? perhaps the registers for timer 8 are written to but I set them up wrong to strobe an output pin? my small code follows. @@@ Directives .thumb @ (same as saying '.code 16') .syntax unified @@@ Equates .equ STACKINIT, 0x20005000 .equ GPIOC_MODER, 0x40020800 .equ GPIOC_AFRL, 0x40020820 .equ TIM8_ARR, 0x4001042C .equ TIM8_CCER, 0x40010420 .equ TIM8_CCMR2, 0x4001041C .equ TIM8_CR1, 0x40010400 .section .text .org 0 @@@ Vectors vectors: .word STACKINIT @ stack pointer value when stack is empty .word _start + 1 @ reset vector (manually adjust to odd for thumb) .word _nmi_handler + 1 @ .word _hard_fault + 1 @ .word _memory_fault + 1 @ .word _bus_fault + 1 @ .word _usage_fault + 1 @ _start: ldr r0, = GPIOC_MODER @ this sets the pin to alternate function ldr r1, = 0x00020000 @ this sets the pin to alternate function str r1, [r0] @ this sets the pin to alternate function ldr r0, = GPIOC_AFRL @ this sets the pin to alternate function ldr r1, = 0x00030000 @ this sets the pin to alternate function str r1, [r0] @ this sets the pin to alternate function ldr r0, = TIM8_ARR @ this sets maximum count in the timer ldr r1, = 0x02625A00 @ this sets maximum count in the timer str r1, [r0] @ this sets maximum count in the timer ldr r0, = TIM8_CCER @ this sets maximum count in the timer ldr r1, = 0x0100 @ this sets maximum count in the timer str r1, [r0] @ this sets maximum count in the timer ldr r0, = TIM8_CCMR2 @ this sets maximum count in the timer ldr r1, = 0x0100 @ this sets maximum count in the timer str r1, [r0] @ this sets maximum count in the timer ldr r0, = TIM8_CR1 @ this sets maximum count in the timer ldr r1, = 0x0001 @ this sets maximum count in the timer str r1, [r0] @ this sets maximum count in the timer loop: add r0, 1 add r1, 2 add r2, 3 add r3, 4 add r4, 5 b loop @ continue forever _dummy: @ if any int gets triggered, just hang in a loop _nmi_handler: _hard_fault: _memory_fault: _bus_fault: _usage_fault: add r0, 1 add r1, 1 b _dummy #peripheral-timer-memory-error2013-08-06 1:34 PM
You must enable the AHBx and APBx clocks for the peripherals you wish to use.
ie APB2ENR and SYSCFGLDR R0, =0x40023844 ; RCC_APB2ENR
LDR R1, =0x00004000 ; ENABLE SYSCFG CLOCK
STR R1, [R0, #0]
2013-08-06 2:06 PM
ldr r0, =0x40023800 ; RCC
ldr r1, =4 ; RCC_AHB1ENR_GPIOCEN
ldr r2, [r0, #0x30] ; RCC_AHB1ENR
orr r2, r1
str r2, [r0, #0x30]
ldr r1, =2 ; RCC_APB2ENR_TIM8EN
ldr r2, [r0, #0x44] ; RCC_APB2ENR
orr r2, r1
str r2, [r0, #0x44]
; OR
ldr r0, =0x40023800 ; RCC
ldr r1, [r0, #0x30] ; RCC_AHB1ENR
orr r1, r1, #4 ; RCC_AHB1ENR_GPIOCEN
str r1, [r0, #0x30]
ldr r1, [r0, #0x44] ; RCC_APB2ENR
orr r1, r1, #2 ; RCC_APB2ENR_TIM8EN
str r1, [r0, #0x44]
2013-08-06 2:19 PM
Thanks for the reply. I'll try it; however; I am further confused. When I look at your assignment for the RCC register, I get the impression you are setting bit 13, which is reserved. I would expect you want to set bit 1 which is timer 8. I expect 0x0002.
Is my concept of byte order wrong?2013-08-06 3:14 PM
We're talking about the F4, right?