2024-05-28 5:32 AM
Hello!
I'm following the STM32 tutorial on External interrupts from here and got stuck.
The controller doesn't react to the press of button and the IDE for some reason switched to tab of `startup_stm32h503rbtx.s`.
Reproducing steps:
1. Create a new project (STM32 Project)
2. Select Nucleo H503 as target board
3. Go to PinOut and configuration, change mode of PC13 to GPIO_EXTI13
4. Go to GPIO tab, select mode External Interrupt with Falling edge, without Pull-up ot Pull-down, set user label to B1
5. Go to NVIC tab and enable `EXTI Line 13 interrupt`, press `Ctrl + S`
6. Go to section user Code 4 of main.c and insert the following function into it:
/* USER CODE BEGIN 4 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
if(GPIO_Pin == GPIO_PIN_13) {
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
} else {
__NOP();
}
}
/* USER CODE END 4 */
7. Save and run
Used parts:
- board: Nucleo64-H503
- IDE : Stm32CubeIDe 1.15.1
- STLink Firmware: V3.J15.M6
Solved! Go to Solution.
2024-05-28 7:29 AM
Hello @username007,
As you are configuring the PC13 as External Interrupt with Falling edge, in the callback, use HAL_GPIO_EXTI_Falling_Callback function instead of HAL_GPIO_EXTI_Callback as it's not the same API as in the STM32L4
You can check the available EXTI callbacks in stm32h5xx_hal_gpio.c, there are:
* HAL_GPIO_EXTI_Falling_Callback
* HAL_GPIO_EXTI_Rising_Callback
* HAL_GPIO_EXTI_IRQHandler
This should work now!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-28 7:29 AM
Hello @username007,
As you are configuring the PC13 as External Interrupt with Falling edge, in the callback, use HAL_GPIO_EXTI_Falling_Callback function instead of HAL_GPIO_EXTI_Callback as it's not the same API as in the STM32L4
You can check the available EXTI callbacks in stm32h5xx_hal_gpio.c, there are:
* HAL_GPIO_EXTI_Falling_Callback
* HAL_GPIO_EXTI_Rising_Callback
* HAL_GPIO_EXTI_IRQHandler
This should work now!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-28 7:36 AM
Thank you!
P.S. I have no idea why it works NOW, but I tried that already and that didn't work before.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.