Can't get the STM32H753 ADC to work with DMA in cubemx
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-19 6:45 AM
I try to configure ADC + DMA continues cicrcular mode for a H753eval board with CubeMX but with no success.
The example en.stm32cubeh7\STM32Cube_FW_H7_V1.2.0\Projects\STM32H743I_EVAL\Examples\ADC\ADC_DMA_Transfer works perfect but as I have started using cubemx for my other peripherals I would like to stay with cubemx, but I don't get it to work with the ADC+DMA.
Now I have backed to a completely clean project for a 753XI, only configured ADC1_IN0 and RCC(25MHz->400MHz sysclk and 18.75MHz ADC clk).
When I run it as ADC con't mode without DMA
and add the following to my main.c, everything works.
#include ''main.h''
#include ''stm32h7xx_hal.h''ADC_HandleTypeDef hadc1;
uint16_t adcData;
void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_ADC1_Init(void);int main(void)
{ HAL_Init();SystemClock_Config();
MX_GPIO_Init();
MX_ADC1_Init();HAL_ADC_Start(&hadc1); while (1) { adcData = HAL_ADC_GetValue(&hadc1);But when I change ADC1 config in cubemx to:
added a DMA1 stream0, with circular mode and changed the rows in my code to:
ALIGN_32BYTES (static uint16_t adcData[32] );
HAL_ADC_Start_DMA(&hadc1,(uint32_t*)adcData,32)
and no code in main()
Nothing works! If a check adc.dr register with the debugger it only takes one value at start-up and nothing more.
I've also fiddled with the Conversion Data Management mode as that parameter is a little unclear to me, circular mode is set in the DMA tab as well and the youtube clips I have seen is using older parts/version which doesn't have that setting.
I've also tried for hours to compare the code generated with the one in the Project/__ /Example to find the problem but without success.
using cubemx 4.25.0
Some ideas anyone??
Thx / Martin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-20 2:45 AM
Solution found: cubemx, at least for H753 and EWARM generates 0x20000000 as default RAM area in the linker file(stm32h753xx_flash.icf) and that is the DTCM-RAM which is not accessible from the standard DMA.
Where is the ICF editor referred to below, I did edit the file for now!
/*###ICF### Section handled by ICF editor, don't touch! ****/
/*-Editor annotation file-*//* IcfEditorFile='$TOOLKIT_DIR$\config\ide\IcfEditor\cortex_v1_0.xml' *//*-Specials-*/define symbol __ICFEDIT_intvec_start__ = 0x08000000;/*-Memory Regions-*/define symbol __ICFEDIT_region_ROM_start__ = 0x08000000;define symbol __ICFEDIT_region_ROM_end__ = 0x081FFFFF;/*define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;define symbol __ICFEDIT_region_RAM_end__ = 0x2001FFFF;*/define symbol __ICFEDIT_region_RAM_start__ = 0x24000000;define symbol __ICFEDIT_region_RAM_end__ = 0x2407FFFF;define symbol __ICFEDIT_region_ITCMRAM_start__ = 0x00000000;define symbol __ICFEDIT_region_ITCMRAM_end__ = 0x0000FFFF;/*-Sizes-*/define symbol __ICFEDIT_size_cstack__ = 0x400;define symbol __ICFEDIT_size_heap__ = 0x200;/**** End of ICF editor section. ###ICF###*/define memory mem with size = 4G;define region ROM_region = mem:[from __ICFEDIT_region_ROM_start__ to __ICFEDIT_region_ROM_end__];define region RAM_region = mem:[from __ICFEDIT_region_RAM_start__ to __ICFEDIT_region_RAM_end__];define region ITCMRAM_region = mem:[from __ICFEDIT_region_ITCMRAM_start__ to __ICFEDIT_region_ITCMRAM_end__];define block CSTACK with alignment = 8, size = __ICFEDIT_size_cstack__ { };
define block HEAP with alignment = 8, size = __ICFEDIT_size_heap__ { };initialize by copy { readwrite };
do not initialize { section .noinit };place at address mem:__ICFEDIT_intvec_start__ { readonly section .intvec };
place in ROM_region { readonly };
place in RAM_region { readwrite, block CSTACK, block HEAP };- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-20 6:40 AM
>>the DTCM-RAM which is not accessible from the standard DMA.
Diagramming suggest the plumbing is there, and the DTCM-RAM is viable for SDMMC DMA operation, which is less problematic from a caching/sharing/coherency standpoint
Up vote any posts that you find helpful, it shows what's working..