cancel
Showing results for 
Search instead for 
Did you mean: 

Can't get ADC values

Epsilon03
Associate II

I have an STM32G474RE, I have not used any HAL or LL libraries, I have only programmed using the registers, my issue is that I am only getting 0 on the output of the ADC, I read through the reference manual and still couldn't solve the problem. I have used ADC channel 1 and PA0 pin since that is what was written in the manual. The output from the UART is shown below.

Thank you in advance for giving me your attention !!


_legacyfs_online_stmicro_images_0693W00000dDeuQQAS.png 

#include "stm32g4xx.h"

#include <stdio.h>

void adc_calib(void);

void adc_init(void);

void adc_conversion(void);

uint32_t adc_read(void);

void adc_init(void)

{

//Enable Debugging LED

RCC->AHB2ENR |=(1U<<0);

GPIOA->MODER |=(1U<<10);

GPIOA->MODER &=~(1U<<11);

//Set PA0 to analog mode

GPIOA->MODER |=(1U<<0)|(1U<<1);

//Enable clock access to ADC12

RCC->AHB2ENR |=(1U<<13);

//Setting CK MODE to adc_hclk/4 (Synchronous clock mode)

ADC12_COMMON ->CCR |=(1U<<16);

ADC12_COMMON ->CCR |=(1U<<17);

//Setting PRE Scaler to 0100: input ADC clock divided by 8

ADC12_COMMON ->CCR &=~(1U<<18);

ADC12_COMMON ->CCR &=~(1U<<19);

ADC12_COMMON ->CCR |= (1U<<20);

ADC12_COMMON ->CCR &=~(1U<<21);

//Disabling ADC from DEEP PWD

ADC1->CR &=~(1U<<29);

//Enabling ADVERGEN

ADC1->CR |=(1U<<28);

//Waiting

for(int i=0;i<1000000;i++)

{

}

}

void adc_calib(void)

{

//Disabling ADEN

ADC1->CR &=~ (1U<<0);

//Disabling ADCALIF

ADC1->CR &=~ (1U<<30);

//Enabling ADCAL

ADC1->CR |= (1U<<31);

//Waiting for ADCAL to finish calibrating

while((ADC1->CR & (1U<<31))!=0)

{

}

//Enabling ADEN

ADC1->CR |=(1U<<0);

}

void adc_conversion(void)

{

//Disabling ADSTART

ADC1->CR &=~(1U<<2);

//Setting length to (0000: 1 conversion)

ADC1->SQR1 &=~(1U<<0);

ADC1->SQR1 &=~(1U<<1);

ADC1->SQR1 &=~(1U<<2);

ADC1->SQR1 &=~(1U<<3);

//Setting priority 1 to Channel 1 (0001)

ADC1->SQR1 |= (1U<<6);

//Setting Sampling time to 12.5 ADC clock cycles (010)

ADC1->SMPR1&=~(1U<<6);

ADC1->SMPR1|= (1U<<7);

ADC1->SMPR1&=~(1U<<8);

}

uint32_t adc_read(void)

{

//ADC is set to continuous conversion mode

ADC1->CFGR |= (1U<<13);

//Enabling ADSTART

ADC1->CR |=(1U<<2);

//Wait for ADC to start

while(!(ADC1->CR & (1U<<2)))

{

}

//Wait for EOC flag to set

while(!(ADC1->ISR & (1U<<2)))

{

}

//Turn on debugging LED to indicate the program is ready to send data

GPIOA->ODR ^=(1U<<5);

//Read data from DR

return(ADC1->DR);

}

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
S.Ma
Principal

Not verse in STM32G4, however, if you do need to de-clunk the system, use a debug proble such as ST Link, run the code, stop the code, open the watch window and look at the SFR registers of the GPIO and ADC to find out. You may actually manually change some registers then continue the code.... faster than rebuild every itteration.

LCE
Principal II

Although I think it's great that you are writing registers directly, I think it makes sense to use bit defines to make the code more readable.

Not only for us, but also for yourself. Or will you remember in 6 months what bit y of register x means?

Epsilon03
Associate II

Sorry im new to this, I have added comments to each line if that helps, will work on defines and update the code once i complete it.

Sorry im new to this, I have added comments to each line if that helps, will work on "defines" and update the code once i complete it.

I used the stk link debugger, however since there is some issue with my live expressions, I use the UART to display values

ONadr.1
Senior III

I would try to write the entire code using HAL FW and verify its functionality. Then with the help of the debugger find out where, what and how to set.

I wrote the code in HAL and it worked as intended, I need help in figuring out what I am doing wrong.

ONadr.1
Senior III

Run the code in debug mode and watch step by step how the GPIO is set, how the ADC is turned on, how the channel is configured and compare it with your own code. You will see where the difference is and it will be easier to understand the correct sequence of individual steps.