2017-02-09 1:20 PM
Stm32 +wifi plus click
2017-02-10 12:34 AM
Hi
Chhoud.Oussama
,You have to refer to the CubeMX user manual to get started with this tool usage. In this Community as well as
, you may find a set of tutorials and videos to help you.However, to use Wifi, you may check the firmware (
) associated to (Wi-Fi expansion board based on SWPF01SA module for STM32 Nucleo).-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-02-11 2:02 PM
i think im not need
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fecosystems%2Fstm32-open-development-environment%2Fstm32-nucleo-expansion-boards%2Fstm32-ode-connect-hw%2Fx-nucleo-idw01m1.html
because i have a module of Wifi (wifi plus click )2017-02-11 2:09 PM
Look at the USART examples provided with CubeMX. See if you can port or learn anything from the IDW01M1 software/support.
For custom software work you might need to find a consultant/contractor.