cancel
Showing results for 
Search instead for 
Did you mean: 

Can someone help me to write a code in CUbeMX of STM32F4 and connect with wifi plus click ..

chhoud oussama
Associate
Posted on February 09, 2017 at 22:20

Stm32 +wifi plus click

3 REPLIES 3
Amel NASRI
ST Employee
Posted on February 10, 2017 at 09:34

Hi

Chhoud.Oussama

‌,

You have to refer to the CubeMX user manual to get started with this tool usage. In this Community as well as

http://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-configurators-and-code-generators/stm32cubemx.html

, you may find a set of tutorials and videos to help you.

However, to use Wifi, you may check the firmware (

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-software/x-cube-wifi1.html

) associated to

http://www.st.com/content/st_com/en/products/ecosystems/stm32-open-development-environment/stm32-nucleo-expansion-boards/stm32-ode-connect-hw/x-nucleo-idw01m1.html

(Wi-Fi expansion board based on SWPF01SA module for STM32 Nucleo).

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on February 11, 2017 at 22:02

i think im not need

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fecosystems%2Fstm32-open-development-environment%2Fstm32-nucleo-expansion-boards%2Fstm32-ode-connect-hw%2Fx-nucleo-idw01m1.html

because i have a module of Wifi (wifi plus click )

Posted on February 11, 2017 at 23:09

Look at the USART examples provided with CubeMX. See if you can port or learn anything from the IDW01M1 software/support.

For custom software work you might need to find a consultant/contractor.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..