2022-08-24 11:59 PM
This is a question I posted on Reddit a long time ago, but it hasn't been solved yet, so I'm asking here.
I solved the dlc value in the notepad picture.
And there was an error even though I connected the rs pin afterwards.
I want to know the solution to this error code 2097152.
Is there anyone who got the same error as me while using the can protocol?
2022-08-25 12:00 AM
2023-11-30 1:50 AM
Hi @jha g.1 did you get the solution yet?
2023-11-30 3:13 AM
Um, I'm really not sure what is your problem.
So you should conclude them together and ask again.