2017-08-08 1:56 AM
I download the en.stm32cubemx.zip file from st.com website, but can't install it.
When I double-click the SetupSTM32CubeMX-4.22.0.app, nothing happen.
my java version is :
╰─
$
java -version
java version '1.8.0_111'
Java(TM) SE Runtime Environment (build 1.8.0_111-b14)
Java HotSpot(TM) 64-Bit Server VM (build 25.111-b14, mixed mode)
And the system OS is 10.12.6, should be the latest version.
2017-09-14 9:49 PM
I have re-installed the lastest version CubeMX-4.22.1, the installation is OK with the java -jar method. But when I startup the APP, the server-checking can not pass, and it always using lot of cpu. I have disabled my network monitor, but useless...
Any idea for this problem?
在2017年09月13日 15:58,Sirma Siang<st-microelectronics@jiveon.com> 写�:
|
|
STMicroelectronics Community
|
|
Re: can not install stm32cubemx on mac
reply from Sirma Siang in STM32 MCUs Forum - View the full discussion
I am using an up to dated MacOSx machine.
Cube is running fine.
Delete the .app and reinstall it might be a good idea.
Kind regards
Sirma
Reply to this message by replying to this email, or go to the message on STMicroelectronics Community
Start a new discussion in STM32 MCUs Forum by email or at STMicroelectronics Community
Following Re: can not install stm32cubemx on mac in these streams: Inbox
This email was sent by STMicroelectronics Community because you are a registered user.
You may unsubscribe instantly from STMicroelectronics Community, or adjust email frequency in your email preferences
|
|