Skip to main content
mckrek7
Visitor II
December 19, 2020
Question

CAN messages receiver

  • December 19, 2020
  • 0 replies
  • 485 views

Hi,

I tried to do a research but since I'm kinda lost and nothing helped me to clear it I decided to ask here.

 

I got STM32H747i-Disco + MB1280 A-03 (to receive CAN). I designed graphics in TouchGFX, which should act accordingly to CAN messages received. I wrote code for Arduino DUE to transmit messages, conected RX and TX with cables and that's kinda as far as I can go right now.

 

I read some articles about interfacing with touchgfx, where I understood that in model.hpp I should write the receiving part and then decided which function I should call. Is there any library/code for the "model" for my board that I could use or at least be inspired?

 

I already wrote a CAN receiver in python for Raspberry but I don't know how to do it here in Touch GFX.

 

Thank you for every helpful answer in advance.

This topic has been closed for replies.