cancel
Showing results for 
Search instead for 
Did you mean: 

Can LSI oscillator be disabled once the IWDG has started running on STM32G0 ?

Tom MacDonald
Associate III

In my application I have configured IWDG to start running.

I would like to prevent the IWDG from resetting the MCU while in stop 1 mode for extended period of time.

In the reference manual it says: "Once running, the IWDG cannot be stopped."0693W00000QL7NIQA1.png 

But in the RCC section of the manual it says

"The LSI RC can be switched on and off using the LSION bit in the Control/status register (RCC_CSR)."

0693W00000QL7NmQAL.png 

This would lead me to believe that its possible to turn off the LSI clock after the IWDG has been enabled.

If I try to turn off the LSI clock before entering Stop 1 mode, the MCU ends up being reset by the IWDG.

Is it true that LSI cannot be stopped ig IWDG has been engaged?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Hi @Peter BENSCH 

I have the same problem, does Tom right?

set the bit 17 to 0, can stop the IWDG?