2021-01-12 5:53 PM
We use stm32g474re in our project. The i2c devices used in our board have two types, one support high-speed mode while the others doesnot. Currently, i set the i2c master with fast mode(400K). Is it possible to set i2c master with high-speed mode and commuicate with slave in fast mode?
2021-03-25 2:57 AM
Hi KDu.13 (Community Member),
The I2C master set to high-speed mode should communicate only with I2C slaves also set to high-speed mode. In STM32 devices we have I2C supporting Fast mode plus (FM+) mode. High-speed I2C mode is a bit different from fast mode (current source as pull-up, no clock stretching in middle, ... ).
The difference between different I2C modes can be read in a short articles:
https://www.i2c-bus.org/fast-mode-plus/
https://www.i2c-bus.org/highspeed/
https://www.i2c-bus.org/fastmode/
Regards
Igor