Can I Program STM32-Nucleo Boards With Ubuntu-32 bit?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-09-26 6:15 AM
Hi,
I am looking to get started with STM32. When studying, I came around this
http://www.mouser.com/ds/2/389/nucleo-f031k6-973846.pdf
.As seen on Page 2, of this document, I see that it says:
System Requirements:
Windows® OS (XP, 7, 8 and 10), Linux® 64-bit or macOS™
I did read, one more datasheet of another nucleo board and it said the same requirement.
I have access to a 32 bit Ubuntu only. Does it means that my STM32 journey has ended (or vastly limited) before starting ?
In short, do most
STM32
devices require a 64 bit Linux environment?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-09-26 11:10 AM
>>In short, do most
STM32
devices require a 64 bit Linux environment?The devices don't inherently depend on such, just the tools you choose to use.
I can run GCC/GNU ARM cross compilers on 32-bit Linux platforms, most systems from the last decade can run 64-bit Linux.
With mbed you have the Nucleo show up as a USB MSC (flash drive) into which you drop compiled binary code.
Just don't expect commercial entities to expend a lot of resources supporting antiquated/limited hardware.
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
‎2017-09-26 11:44 PM
Umm.. Could you please suggest any one such compiler for my 32 bit Linux?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-09-27 12:50 AM
Rowley (Crossworks for ARM) has a working Linux version.
I am using it for years now, on a 32-bit OS.
Else, either a plain command line toolchain, or a tinker IDE with Eclipse. Several compiler/linker are freely available.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-09-27 3:34 PM
You need to check if stmcube depends upon a 64-bit JVM. (See ST Micro web site).
Other tools required are: gcc/make/gdb and openocd. Most of the commercial products are based on these open source products. I use the open source versions (
) and find they are acceptable. If 32-bit binaries are not available you can create them from the source code.