2019-10-27 04:54 PM
hello, I am using L031K6 with UM1956 board.
I am trying ultra low power sensor project with it.
I want to use this board in disabling USB serial communication port status.
because I think it is spending a lot of battery, even though the CPU is in the sleep mode.
Dose it have this option, or possible way to make it?
thank you for read.
2019-10-28 01:48 AM
You can disable the debugger part altogether by powering the MCU directly from CN4-14 at 3V3. You need to unsolder SB14 and SB9 beforehand. See 6.2.2 paragraph of UM1956 for all available powering schemes details.