cancel
Showing results for 
Search instead for 
Did you mean: 

CAN error 0x000E0000

JBond.1
Senior II

Hi, I have STM32F091RC board and I am using CAN interface to read CAN BUS data from car. CAN works when I am powering STM32 from USB port (U5V). When I try to power STM32 from car (with E5V port), I get error in can interface 0x000E0000.

What could be causing this error?

I tested car 5V adapter, it seems that it is giving ~4.6V instead of exact 5V, could this be the cause?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0