Skip to main content
KMew
Senior III
January 27, 2023
Question

CAN Communication: FD Transceiver with Classic CAN Controller

  • January 27, 2023
  • 1 reply
  • 1178 views

Hello,

I am looking to communicate between my control board and someone else's control board that is already designed via CAN communication. I am only looking to do Classic CAN communication (Not FD). I have the following parts:

MCU on my Control Board: STM32H7B3LIH6Q

MCU on coworkers Control Board: STM32F303RET

CAN Transceiver on both Control Boards: MCP2542WFD-E/SN

The STM32H7 controller can do both CAN 2.0B and CAN FD

The STM32F7 controller can only do CAN 2.0B

The CAN Transceiver, according to the datasheet, is a CAN FD Transceiver

If I want to communicate via CAN 2.0B (Classic CAN) and configure both controllers to Classic CAN, will the following connection scheme work:

STM32H7 -> FD CAN Transceiver -> FD CAN Transceiver -> STM32F7

This topic has been closed for replies.

1 reply

AScha.3
Super User
January 28, 2023

should work perfect; just do not forget termination resistors on connection line.

If you feel a post has answered your question, please click on " Best Answer ".