2021-03-29 07:11 AM
Tried out the example in STM32Cube_FW_F7_V1.16.0 and couldn't get the baudrate to match the description.
Have any body else encounterred this problem?
2021-03-29 08:59 AM
No not specifically, but prior examples for different board/chips have been wrong in the past.
The bit rate is determined by the APB clock the CAN peripheral is attached too, divided by the prescaler, and then divided by the sum of the bit-quanta settings.