cancel
Showing results for 
Search instead for 
Did you mean: 

bypass config with STDPERIPH_DRIVER

mahmoud boroumand
Associate III
Posted on August 17, 2017 at 13:05

hello 

i use stm32f030f4 and use 10MHz oscillator (BYPASS) and i want achieve to 48mhz in mcu.

and i use STDPERIPH_DRIVER and keil v5.what configuration i have to do ?what code i have to add to my project?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on August 17, 2017 at 19:00

RCC_HSEConfig(RCC_HSE_ON); becomes RCC_HSEConfig(RCC_HSE_Bypass); and you don't need to wait for it to start

or something along these lines in system_stm32f0xx.c, called via SystemInit()

static void SetSysClock(void)

{

/******************************************************************************/

/*            HSE BYPASS used as System clock source                          */

/******************************************************************************/

  /* SYSCLK, HCLK, PCLK configuration ----------------------------------------*/

  /* Enable HSE BYPASS */

  RCC->CR |= ((uint32_t)RCC_CR_HSEBYP);

  /* Enable Prefetch Buffer and set Flash Latency */

  FLASH->ACR = FLASH_ACR_PRFTBE | FLASH_ACR_LATENCY;

  /* HCLK = SYSCLK */

  RCC->CFGR |= (uint32_t)RCC_CFGR_HPRE_DIV1;

  /* PCLK = HCLK */

  RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE_DIV1;

  /* Select HSE as system clock source */

  RCC->CFGR = (RCC->CFGR | (uint32_t)((uint32_t)~(RCC_CFGR_SW))) | (uint32_t)RCC_CFGR_SW_HSE;

  /* Wait till PLL is used as system clock source */

  while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)RCC_CFGR_SWS_HSE);

}
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4
Posted on August 17, 2017 at 13:38

You'd need to modify the clock/pll setting code in system_stm32f0xx.c

Not sure the available multiplier and divider settings will get you from 10 MHz to 48 MHz, review the setting options in the reference manual.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on August 17, 2017 at 13:52

If i want get 10MHz to 10 mhz what code i have to add?

i dont know how enable bypass.

Posted on August 17, 2017 at 17:49

Hi,

HSE 10MHz input frequency does not allow you to get the 48MHz SYSCLK with PLL.

HSE PREDIV is between 1 and 16

PLLMul is between 2 and 16

But you can with a HSE frequncy of 8MHz or 12MHz

For 8Mhz PLL Input:

HSE_PREDIV = 1

PLL_MUL = 6

For 12Mhz PLL Input:

HSE_PREDIV = 1

PLL_MUL = 4

BR

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on August 17, 2017 at 19:00

RCC_HSEConfig(RCC_HSE_ON); becomes RCC_HSEConfig(RCC_HSE_Bypass); and you don't need to wait for it to start

or something along these lines in system_stm32f0xx.c, called via SystemInit()

static void SetSysClock(void)

{

/******************************************************************************/

/*            HSE BYPASS used as System clock source                          */

/******************************************************************************/

  /* SYSCLK, HCLK, PCLK configuration ----------------------------------------*/

  /* Enable HSE BYPASS */

  RCC->CR |= ((uint32_t)RCC_CR_HSEBYP);

  /* Enable Prefetch Buffer and set Flash Latency */

  FLASH->ACR = FLASH_ACR_PRFTBE | FLASH_ACR_LATENCY;

  /* HCLK = SYSCLK */

  RCC->CFGR |= (uint32_t)RCC_CFGR_HPRE_DIV1;

  /* PCLK = HCLK */

  RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE_DIV1;

  /* Select HSE as system clock source */

  RCC->CFGR = (RCC->CFGR | (uint32_t)((uint32_t)~(RCC_CFGR_SW))) | (uint32_t)RCC_CFGR_SW_HSE;

  /* Wait till PLL is used as system clock source */

  while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)RCC_CFGR_SWS_HSE);

}
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..