2017-07-05 6:15 AM
I have a P-NUCLEO-IHM001 board and try to build an example from the directotry 'STM32Cube_FW_F3_V1.8.0' with AC6 toolchain and always get a build error 238 on example/user/main.o
Why does this occur and how can I solve it?
2017-07-05 7:50 AM
Hi
raphael.vanstraelen
,Which example did you tested ? Did you make some update on the example ?
Which version of AC6 is used?
RegardsImen
2017-07-06 12:13 AM
Hello Imen,
I did not make any updates on the example. I unzipped the file and installed it in following directory
C:\Program Files (x86)\STMicroelectronics
I imported the directory in system workbench
I used the following example:
C:\Program Files (x86)\STMicroelectronics\STM32Cube_FW_F3_V1.8.0\Projects\STM32F302R8-Nucleo\Templates\SW4STM32\STM32F302R8-Nucleo
AC6 version is
System Workbench for STM32 - OpenOCD (for Windows 32bits)
Version: 1.14.0.201705091103
Build id: @build@Copyright (c) 2014 Ac6 Tools. All rights reserved.
Visit
https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.openstm32.org
2017-07-06 3:24 AM
A bit more information about the error message would be really helpful.
Perhaps your IDE or the project is not set up properly ?
Since an *.o file is involved, it seems to be a linker error.
Some sources not added to the project ?