Skip to main content
Jan Breuer
Associate II
November 14, 2017
Question

[bug] STM32CubeMX 4.23.0 does not copy startup.s

  • November 14, 2017
  • 1 reply
  • 572 views
Posted on November 14, 2017 at 09:44

I have selected option for 'STM32 Firmware Library package' -> 'copy only the necessery library files'.

I'm using just LL libraries and GPDSC project.

All files ware generated without error but no startup file was present in the project, only blank directories 'arm', 'gcc' and 'iar' ware created in directory 'Drivers/CMSIS/Device/ST/STM32F0xx/Source/Templates/'

On the other hand, it copies 'system_stm32f0xx.c' in 'Templates' directory, which is not needed, because similar file is generated with the same name and functionality to the 'Src' directory. 

MCU: STM32F030F4Px

PC OS: Linux

CubeMX version: 4.23.0

Firmware package: STM32Cube FW_F0 V1.9.0

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    November 15, 2017
    Posted on November 15, 2017 at 14:46

    Hello,

    Your issue is raised to CubeMx team for further check and investigation.

    Best Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks