cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in STM32CUBEMX 4.26

CAPOSIENA.Philippe
Associate II
Posted on June 07, 2018 at 09:32

Hello,

i have updated STM32CubeMx from 4.25.1 to 4.26 and now i can no more generate my project. It freezes during the generation project. I uses a STM32L475.

ST, please give me a link to download the 4.25.1 version because i can't find it anymore.

It's very very very urgent !!! My customer will not wait.

I need to do some modifications today. I tried to phone to my ST contacts but i can't join no one.

Thanks.

Philippe

4 REPLIES 4
Nawres GHARBI
ST Employee
Posted on June 07, 2018 at 09:48

Hello Philippe, 

Could you share your ioc please ?

CAPOSIENA.Philippe
Associate II
Posted on June 07, 2018 at 10:23

For the moment i can't share the ioc file because it's confidential. I must try to reproduce the problem with a simple ioc project.

CAPOSIENA.Philippe
Associate II
Posted on June 07, 2018 at 11:46

Hi,

i deleted some files in my TrueStudio project folder and now i can generate the STM32CubeMx project.

The files deleted are :

- .mxproject

- common.ftl

- mw_common.ftl

- usbhconf_l4.ftl

- usbhconf_l4.ftl_save

- folder MXTmpFiles

- 2 old log files

I don't know if it is really the origin of the problem.

Philippe

Posted on June 07, 2018 at 10:24

OK or you can also share the log file it may be helpful too