cancel
Showing results for 
Search instead for 
Did you mean: 

[bug]:CubeMX HAL timebase tick interrupt cleared in NVIC via pin editing

Daniel Hassanian
Associate III
Posted on April 25, 2018 at 11:09

Hello,

I found a bug in the latest version of CubeMX which causes the tick timer for HAL to be cleared in code if the corresponding timer pin is cleared.

Steps to reproduce:

1- Open project with any MCU.

2- Configure SYS to use Timebase source other than systick (here I use TIM14 for STM32F070F6)

3- Check that in NVIC 'Time base: TIMxxGlobal interrupt' should be Enabled(and grayed out)

4- go to pin configuration and set one of the pins that timer uses for the timer output purposes(for TIM14 here we have PB1 TIM14_CH1) and select it. (we can't use the pin because HAL is taking control of the time)

5- reset the pin.

6- the Time base interrupt is now disabled in step 3 which should not happen.

I think sometimes it also happens if you configure the same pin for GPIO input/output but i can't reproduce it.

#stmcube-bug
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Khouloud GARSI
ST Employee
Posted on April 25, 2018 at 12:05

Hello Daniel,

This is highlighted internally for further check. We will keep you posted on any update.

Thanks for sharing your feedback on our STM32MCUs Forum.

Khouloud.

Nawres GHARBI
ST Employee
Posted on April 30, 2018 at 13:06

Hi Daniel, 

Thanks for rising this issue, it will be fixed next release