2010-10-05 11:38 AM
I downloaded the firmware package from here:
http://www.st.com/mcu/modules.php?name=mcu&file=devicedocsmdt&FAM=110&DEV=STM32VLDISCOVERY
When I open the file stm32f10x_an3268_fw.chm, the navigation panel appears to work fine (Contents, Index, Search, Favorites). However, the actual pages do not appear -- instead, I get ''Navigation to the wepage was canceled -- Retype the address''. This happens from two different machines -- workstation and laptop. Anybody else have this issue?2010-10-05 1:27 PM
Seems to work under XP Professional, for the file 981955 bytes, 9/13/2010
Same file fails in manner described in Vista2010-10-06 10:40 AM
I get the same thing when trying to open the chm file from a network share. If you are too, try copying the file to your 'C' drive. (Works for me) I can get it to work from a USB stick too. I'm running XP Pro SP3.
2010-11-04 8:34 PM
right click and go to the proprties of the file, look at read only, security, advanced ...
it worked for me2010-11-05 12:51 AM
I think this is a known issue with .chm files - see:
[DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/FYI Problems with STM32 Help Files (.chm) and Keil uVision&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E¤tviews=149]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fARM%20CortexM3%20STM32%2fFYI%20Problems%20with%20STM32%20Help%20Files%20%28%2echm%29%20and%20Keil%20uVision&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E¤tviews=149 See also: