cancel
Showing results for 
Search instead for 
Did you mean: 

Bootloader USB settings

mathilde
Associate
Posted on April 13, 2015 at 12:11

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
jeff2
Associate
Posted on June 06, 2015 at 06:24

Hello,

  I'm curious if you resolved this issue?   I am debugging the same problem on an stm32L0.  

  I used stmCube to create a DFU image which I have flashed and the device does appear in DFU mode.

 

 dfu-util -l outputs the following:

Found DFU: [0483:df11] ver=0200, devnum=35, cfg=1, intf=0, alt=0, name=''UNKNOWN'', serial=''00000000001A''

 However, when I try to actually flash I get the same message:

dfu-util: Could not read name, sscanf returned 0

I've tracked down why this is happening and why the string is ''UNKNOWN'' but I'm trying to understand why it is happenning. 

If I do lsb -v I get this info(trimmed)

    Interface Descriptor:

      bLength                 9

      bDescriptorType         4

      bInterfaceNumber        0

      bAlternateSetting       0

      bNumEndpoints           0

      bInterfaceClass       254 Application Specific Interface

      bInterfaceSubClass      1 Device Firmware Update

      bInterfaceProtocol      2

      iInterface              6

The key here is the last line, 'iInterface 6'.  I have read this is supposed to be the index of the interface name. 

dfu-util calls the libusb function to get the name:

                if (intf->iInterface != 0)

                    ret = libusb_get_string_descriptor_ascii(devh,

                        intf->iInterface, (void *)alt_name, MAX_DESC_STR_LEN);

where intf->iInterface is 6.

This ends up running the following function in the stm32 firmware:

static void USBD_GetDescriptor(USBD_HandleTypeDef *pdev ,

                               USBD_SetupReqTypedef *req)

<snip>

case USB_DESC_TYPE_STRING:

    switch ((uint8_t)(req->wValue))

    {

    case USBD_IDX_INTERFACE_STR:

      pbuf = pdev->pDesc->GetInterfaceStrDescriptor(pdev->dev_speed, &len);

      break;

    default:

#if (USBD_SUPPORT_USER_STRING == 1)

      pbuf = pdev->pClass->GetUsrStrDescriptor(pdev, (req->wValue) , &len);

      break;

#else      

       USBD_CtlError(pdev , req);

      return;

#endif   

static void USBD_GetDescriptor(USBD_HandleTypeDef *pdev ,

                               USBD_SetupReqTypedef *req)

So for me,  the lower byte of req->wValue is 6 but the value ofUSBD_IDX_INTERFACE_STR is 0x5.   So the incoming request for theinterace name always gets an error and thus dfu-util fails. 

Also it look like dfu-util expects the name in a specific format for dfuse devices:

ret = sscanf(intf_desc, ''@%[^/]%n'', name, &scanned);

if (ret < 1) {

free(name);

warnx(''Could not read name, sscanf returned %d'', ret);

return NULL;

}

And the name generated by Cube doesn't match that format:

#define USBD_INTERFACE_STRING_FS     ''DFU Interface''

  So I've got a couple more things to dig into but wanted to see if you found anything while debugging this issue.

  

thanks,

jeff

alex239955_stm1_st
Associate
Posted on November 08, 2015 at 14:30

Were you able to find a solution for this?

I also think it has something to do with the name='UNKOWN' .

(when using dfu-utils 0.5 it says name='UNDEFINED'  ) .

I've seen other devices where it usually has the format  name=''@Some name''  . 

Is there any workaround for this? 

   

johannes23
Associate II
Posted on November 09, 2015 at 11:35

The STM32F42x DFU bootloader in ROM violates the USB spec, according to WireShark and TotalPhase Beagle, causing an issue with libUSB. DFU-util is fine.

Here's a patch for libusb-1.0.19:

https://github.com/axoloti/axoloti/blob/master/platform_osx/src/libusb.stdfu.patch

This workaround works on Windows, OSX and Linux.