2009-08-11 08:15 AM
BOOT0 pin
2011-05-17 04:20 AM
Hi All
Is it possible to use BOOT0 (pin 60 of 64pin package)like general IO pin input? Thank you :-[2011-05-17 04:20 AM
Obviously not, the explanation lies in the pin name itself ''BOOT0''. It's dedicated to serve a predefined hardware behaviour on chip and is well documented in the specifications.
Perhaps looking for 100-pins target if you're running low on free GPIOs ;) cheers Guy2011-05-17 04:20 AM
No.