cancel
Showing results for 
Search instead for 
Did you mean: 

BOOT0 pin

jedlb
Associate II
Posted on August 11, 2009 at 17:15

BOOT0 pin

3 REPLIES 3
jedlb
Associate II
Posted on May 17, 2011 at 13:20

Hi All

Is it possible to use BOOT0 (pin 60 of 64pin package)like general IO pin input?

Thank you :-[

guyvo67
Associate II
Posted on May 17, 2011 at 13:20

Obviously not, the explanation lies in the pin name itself ''BOOT0''. It's dedicated to serve a predefined hardware behaviour on chip and is well documented in the specifications.

Perhaps looking for 100-pins target if you're running low on free GPIOs ;)

cheers

Guy

swhite
Associate III
Posted on May 17, 2011 at 13:20

No.