Board-To-Board abstraction protocol (MUX, eRPC..)
Hi Folks
I'm running a design where i have a sort "Expansions" board where all the Analog inputs and RS485 / UARTS port are located.
This board is running a STM32F107 mcu.
Then i have another board running a STM32F429NIH6 MCU, where we handle LCDs, ETH, External Flash & RAM.
The two boards are connected over a SPI-BUS.
The brain of the system is located on the STM32F429, and we can think the F107 is just a "smart" I/O Expansion. I was looking at a sort of abstraction layer which can "simplify" the dialog between the two boards in the more versatile way.
I have some idea in mind, but i'm not sure i'm on the right way:
Before doing all the exchange protocol myself, i would prefer some stable architecture/system.
- MUX (used in automotive industries). So far i did not find a good implementation online
- eRPC (https://github.com/EmbeddedRPC/erpc)
Any suggestion from your side?