cancel
Showing results for 
Search instead for 
Did you mean: 

bit definitions

walter1
Associate
Posted on July 03, 2008 at 05:23

bit definitions

2 REPLIES 2
walter1
Associate
Posted on May 17, 2011 at 12:39

With help of a little program i made, a lot of regular expressions and some handwork, i extraced the bitnames and places from the datasheet. (see Attachment)

This was neccessary as i prefere direct register banging instead of using high level firmware routines.

Would be nice to get some feedback.

regards,

Walter

[ This message was edited by: walter1 on 03-07-2008 00:32 ]

disirio
Associate II
Posted on May 17, 2011 at 12:39

Very useful, thank you. I also prefer to work at register level and something like this was really needed.

---

ChibiOS/RT

http://chibios.sourceforge.net