cancel
Showing results for 
Search instead for 
Did you mean: 

Basic circuit for programming with STM32F4-Discovery´s STLINK SWD

javi0034
Associate
Posted on May 25, 2014 at 17:49

Hi! I am having problems to program a STM32F107 with the STM32F4-Discovery�s STLINK SWD. I�m wondering I have forgot something very essential.

This is the circuit I've mounted:

0690X00000605SVQAY.png

And these the errors I get:

0690X00000605EsQAI.png

0690X00000605QOQAY.png

0690X00000605NKQAY.png

What I have done:

  • Check the connections
  • Check the supply
  • Start in the 3 different modes: Normal, Hot Plug, Connect Under Reset
  • Update Stlink firmware

Any idea what could be the problem? What is missing? I guess it must be something obvious but I don't see it :(

Thanks

#stm32f4-discovery-stlink-swd
2 REPLIES 2
Posted on May 25, 2014 at 18:29

Check that you have the pin orientation correct.

https://community.st.com/0D50X00009Xka68SAB

 Check that you have disconnected the F4 part from the ST-LINK, via jumpers and solder-bridges are required.I'd have a pull up on the reset, and bulk capacitors on the supplies.If it were my design I'd double check the pin#

Edit: Fixed DEAD LINK, original post from 25-May-2014

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
javi0034
Associate
Posted on May 25, 2014 at 19:25

Thank you. I'm afraid the problem is the orientation!!!