2015-02-08 3:59 PM
I am new to the CAN bus and have spent the last few days looking over code examples and searching the web for tips and I'm using the STM32303C-EVAL board.
I'm just trying to get transmit to work, so my question is this: with nothing connected on the CAN bus DB9, shouldn't I see at least some o-scope activity on the CANH or CANL signals on the bus side of the transceiver? I also have a Microchip CAN bus analyzer that can receive as well as transmit. Thanks, DT #can2015-02-09 2:38 PM
Problem solved and the answer is yes, you can see pulses on the CAN bus with absolutely nothing else connected. The problem was that I was using GPIO_AF_9 instead of GPIO_AF_7. I can transmit and receive (using the Microchip bus analyzer in transmit mode) at 1 Mbps.