cancel
Showing results for 
Search instead for 
Did you mean: 

B-CAMS-OMV Camera Module

Hoodand
Visitor

AE07BDA9850A7DBC0ECCF914D3DC2886.jpg

 

 

 

 

 

 

 

 

 

 

Is my camera module working fine (all 3 LEDs light up)? I am working with the model zoo image classification project, and facing issue.I have 

1 REPLY 1
Julian E.
ST Employee

Hello @Hoodand ,

 

Can you unplug/plug your camera again to see if it helps?

If not, look at the accepted answer in this thread: Solved: STM Model Zoo - STMicroelectronics Community:

  1. Download the .zip file with the .elf inside
  2. Follow the step explained about the elf and STM32CubeProgramer

 

You will see in the second attachment of the post author that he had a similar issue

If it doesn't work, it probably means that a part of the setup does not work like him. Do you have another DISCO board and Camera?

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.