cancel
Showing results for 
Search instead for 
Did you mean: 

Audio streaming clock sync

ajgboomer
Associate III
Posted on February 13, 2013 at 17:00

I am interested in techniques for synchronizing the STMF4 I2S clock with an incoming audio stream on the USB. The clock on the source and the clock on the STM32 board will always be slightly out of sync causing either its DMA to the codec to be ahead or behind the stream. Dropping / stuffing samples or re-sampling the stream are not preferred solutions.

Thanks,

Tony

#stm32f4-i2s #streaming
This discussion is locked. Please start a new topic to ask your question.
33 REPLIES 33
romanetz4
Associate II
Posted on November 07, 2015 at 07:32

And the remain part of quiz.

static uint8_t  usbd_audio_IN_Incplt (void  *pdev)

{

if ((SOF_num>((1<<SOF_RATE)-1))&&flag)

  {flag=0;

  DCD_EP_Flush(pdev,AUDIO_IN_EP);

  };

return USBD_OK;

}

romanetz4
Associate II
Posted on November 09, 2015 at 18:27

I've been working on the Isoc incomplete issue... And got pretty good idea, which solved this problem. At the isoc incomplete interrupt, I mark the current pid (last bit of frame number). At the SOF interrupt, I test if current frame has the same parity, and when it's true, transmit the feedback endpoint data. This way is 100% working.

static uint8_t  usbd_audio_IN_Incplt (void  *pdev)

{

//This ISR is executed every time when IN token received with ''wrong'' PID. It's necessary

//to flush IN EP (feedback EP), get parity value from DSTS, and store this info for SOF handler.

//SOF handler should skip one frame with ''wrong'' PID and attempt a new transfer a frame later.

USB_OTG_DSTS_TypeDef  FS_DSTS;

 FS_DSTS.d32 = USB_OTG_READ_REG32(&(((USB_OTG_CORE_HANDLE*)pdev)->regs.DREGS->DSTS));

 dpid=(FS_DSTS.b.soffn)&0x1;

if (flag)

  {flag=0;

  DCD_EP_Flush(pdev,AUDIO_IN_EP);

  STM_EVAL_LEDToggle(LED4);

  };

return USBD_OK;

}

 

static uint8_t  usbd_audio_SOF (void *pdev)

{     uint8_t res;

static uint16_t n;

USB_OTG_DSTS_TypeDef  FS_DSTS;

  /* Check if there are available data in stream buffer.

    In this function, a single variable (PlayFlag) is used to avoid software delays.

    The play operation must be executed as soon as possible after the SOF detection. */

if (usbd_audio_AltSet==1)

{

if (PlayFlag)

  {

gap=(IsocOutWrPtr-IsocOutRdPtr);

tmpxx=(DMA1_Stream7->NDTR);

if (gap<0) gap+=(AUDIO_OUT_PACKET * OUT_PACKET_NUM);

dgap=gap+tmpxx;

  };

accum+=(TIM2->CCR1);

SOF_num++;

if (SOF_num==(1<<SOF_RATE))

{if (SOF_RATE>6)

{feedback_data+=accum>>(SOF_RATE-6);}

else

{feedback_data+=accum<<(6-SOF_RATE);};

feedback_data>>=1;

SOF_num=0;

accum=0;

}

if ((!flag))

{

FS_DSTS.d32 = USB_OTG_READ_REG32(&(((USB_OTG_CORE_HANDLE*)pdev)->regs.DREGS->DSTS));

if (((FS_DSTS.b.soffn)&0x1) == dpid)

{

DCD_EP_Tx (pdev, AUDIO_IN_EP, (uint8_t *) &feedback_data, 3);

flag=1;

};

};

  }

return USBD_OK;

}

The code in IN handler is the same. This scheme detects right PID and always sends feedback data.
jmf1
Senior
Posted on August 01, 2016 at 15:00

First of all, I would like to thanks Roman to have shared all the above code.

I'm trying, for a DIY audio project, to set-up an Async USB interface from PC to stm32, with feedback endpoint. Would there be some a ''complete example'' of such thing somewhere ?

I have only little experience of USB. I succeeded to get the CubeMX audio standalone application, but I definitly need the feedback EP definition and associated code.

Best regards,

JMF

kim_t26
Associate
Posted on August 31, 2016 at 11:29

Hi,

Did you ever find a complete example including Romans code? 

I would be nice to know which file version Roman has modified.

The usbd_audio_core.c version I have is this:

file    usbd_audio_core.c

author  MCD Application Team

version V1.1.0

date    19-March-2012

/Kim

 

From: fourneron.jean_marc

Posted: Monday, August 01, 2016 3:00 PM

Subject: Audio streaming clock sync

First of all, I would like to thanks Roman to have shared all the above code.

I'm trying, for a DIY audio project, to set-up an Async USB interface from PC to stm32, with feedback endpoint. Would there be some a ''complete example'' of such thing somewhere ?

I have only little experience of USB. I succeeded to get the CubeMX audio standalone application, but I definitly need the feedback EP definition and associated code.

Best regards,

JMF