2008-06-29 05:41 AM
Audio Decoding with STM32
2011-05-17 03:38 AM
Hi all,
Did anyone ported an MP3, WMA or any other high quality decoder in software with STM32, this is just for fun not for a commercial use and to see if STM32 is able to do it and how many MIPS this will take to others control tasks, I see that someone did a a port to STR9 (ARM966), is that port is fully compatble with Thumb-2 instruction set of Cortex-M3 ? Also if some kind of ADPCM or Telephony (skype like) encoding/decoding is also available for toys/games. Thank you ! Bye. Magigimix. 😉