cancel
Showing results for 
Search instead for 
Did you mean: 

Are the 6 fast channels on an STM32h742 ADC preconfigured by default as fast or I need to configure them as fast?

EEtxe.1
Associate II

I have the package LQFP100, so the Application Note specifies that there are 3 fast channels, but the Reference Manual says that the first 6 input channels are fast channels. How is this? If I have to configure them as fast how can I do it or where can I have a look at how is it done?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0