cancel
Showing results for 
Search instead for 
Did you mean: 

Archive of old versions CubeMX

dstindl9
Associate II
Posted on December 09, 2016 at 16:53

Hello,

short question:

Is there link to older versions of CubeMX? Atleast 4.16 or 4.17 version...

I have naively made update from CubeMX 4.16 to 4.18 without a back/up and now I'm unable to compile generated project in our favorite development environment.

Thanks,

Dan

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Lawliet KG
Associate III
Posted on December 09, 2016 at 17:17

Hi Leinad,

No, ST keeps always the last version of CubeMX since it contains bug fixes and some enhancements.

Hoping that ST team provides a list for the previous versions in the future.

Best regards,

Lawliet.

Jeanne Joly
Senior III
Posted on January 23, 2017 at 11:16

Hello Leinad and Lawliet KG,

Indeed, it is not possible to get back to an older version unless you kept it on your computer.

We did not plan to make this feature available.

BTW, it is possible to have serveral different versions on your computer, so don't hesitate to save the different CubeMX versions on which you worked.

BR. Eric

Sirma Siang
ST Employee
Posted on February 01, 2017 at 15:58

Hello Leinad,

Upgrading to 4.18, or 4.19, does not impact the compilation itself.

Could you please elaborate a bit on the compilation error you are facing ?

Could you describe your environnment.. which IDE, which OS ?

Thanks in advance.

Kind regards

Sirma

Posted on June 25, 2017 at 19:02

From my experience working with CubeMX since the day 1 there were cases where the new CubeMX (supposed to be the latest & greatest) was buggy and I had to run older version.

So I think that the older versions should be available for some time - NOT for the user who just upgraded from older version because they have it stored on the PC BUT for new users who just started using CubeMX and were not lucky coming accros newly introduced bug.

See for example this bug where the HSE fails:

https://community.st.com/0D50X00009XkY7sSAF

sarp daltaban
Associate II

There are problems on the SDIO library for the last version and I need STMCubeMX v4.21, for the reference watch first 30 seconds of the tutorial provided below:

https://www.youtube.com/watch?v=0NbBem8U80Y

Expand the Best Answer here, there is a comprehensive list

https://community.st.com/s/question/0D50X00009XkYVDSA3/please-provide-a-way-to-download-older-version-of-the-cube

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..