2016-01-10 11:25 PM
Hi all,
I've some problem with APB1, APB low speed prescaler setting. File stm32f30x.h of STM32F3-Discovery_FW_V1.1.0\Libraries, reports the below PPRE1 meaningin according with DM00043574 pg. 142:#define RCC_CFGR_PPRE1_DIV1 ((uint32_t)0x00000000) /*!< HCLK not divided */
#define RCC_CFGR_PPRE1_DIV2 ((uint32_t)0x00000400) /*!< HCLK divided by 2 */
#define RCC_CFGR_PPRE1_DIV4 ((uint32_t)0x00000500) /*!< HCLK divided by 4 */
#define RCC_CFGR_PPRE1_DIV8 ((uint32_t)0x00000600) /*!< HCLK divided by 8 */
#define RCC_CFGR_PPRE1_DIV16 ((uint32_t)0x00000700) /*!< HCLK divided by 16 */
I've tried to set all the PPRE1 values in SetSysClock() and measured with my scope, and I see that:
RCC_CFGR_PPRE1_DIV1 HCLK not divided
RCC_CFGR_PPRE1_DIV2 HCLK not divided
RCC_CFGR_PPRE1_DIV4 HCLK divided by 2
RCC_CFGR_PPRE1_DIV8 HCLK divided by 4
RCC_CFGR_PPRE1_DIV16 HCLK divided by 8
Have you aver seen the same behavior?
#setsysclock #stm32-mco-clock-output
2016-01-11 01:40 AM
How your measurment look?
Probably you are doing something wrong.2016-01-11 04:27 AM
I'll post the code ASAP.
2016-01-11 11:32 PM
Here below the code, thanks for helping:
#include ''stm32f30x.h''
#include ''main.h''
void
RCC_Configuration(
void
)
{
RCC_ClockSecuritySystemCmd(ENABLE);
/* Enable GPIO clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
//see DM00068049 pg. 235
/* Enable MCO */
RCC_MCOConfig(RCC_MCOSource_SYSCLK);
}
/**************************************************************************************/
void
GPIO_Configuration(
void
)
{
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_DeInit(GPIOA);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_0);
// MCO
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
}
int
main(
void
)
{
/* TIM3_CLK = PCLK1 (APB1_PRESC = 1) = 8Mhz //it seems that APB1_PRESC: any value assigned to RCC_PPRE1 as the same effect of RCC_PPRE1 = RCC_CFGR_PPRE1_DIV1 (no div)
PCLK1 = SYSCLK/1 (AHB_PRESC = 0) = 8Mhz
SYSCLK = PLLCLK = 8Mhz
PLLCLK = PLL_IN * 2 = 8Mhz
PLL_IN = HSE/2 = 4MHz (RCC_CFGR_PLLXTPRE_PREDIV1_Div2 clock divided by 2 for PLL entry)
HSE = 8Mhz USE CLOCK FROM MCO OF ST-LINK*/
RCC_Configuration();
GPIO_Configuration();
while
(1){
}
}
static
void
SetSysClock(
void
)
{
__IO uint32_t StartUpCounter = 0, HSEStatus = 0;
/* HSE oscillator bypassed with external clock */
RCC->CR |= (uint32_t)(RCC_CR_HSEON | RCC_CR_HSEBYP);
/* Wait till HSE is ready and if Time out is reached exit */
do
{
HSEStatus = RCC->CR & RCC_CR_HSERDY;
StartUpCounter++;
}
while
((HSEStatus == 0) && (StartUpCounter != HSE_STARTUP_TIMEOUT));
if
((RCC->CR & RCC_CR_HSERDY) != RESET)
{
HSEStatus = (uint32_t)0x01;
}
else
{
HSEStatus = (uint32_t)0x00;
}
if
(HSEStatus == (uint32_t)0x01)
{
/* Enable Prefetch Buffer and set Flash Latency */
FLASH->ACR = FLASH_ACR_PRFTBE | FLASH_ACR_LATENCY_1;
/* HCLK = SYSCLK */
RCC->CFGR |= (uint32_t)RCC_CFGR_HPRE_DIV1;
/* PCLK2 = HCLK */
RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE2_DIV1;
/* PCLK1 = HCLK */
RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE1_DIV4;
/* PLL configuration: PLLCLK = HSE * RCC_CFGR_PLLMULLx */
RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_PLLSRC | RCC_CFGR_PLLXTPRE | RCC_CFGR_PLLMULL));
RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLSRC_HSI_Div2 | RCC_CFGR_PLLXTPRE_PREDIV1_Div2 | RCC_CFGR_PLLMULL2);
/* Enable PLL */
RCC->CR |= RCC_CR_PLLON;
/* Wait till PLL is ready */
while
((RCC->CR & RCC_CR_PLLRDY) == 0)
{
}
/* Select PLL as system clock source */
RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW));
RCC->CFGR |= (uint32_t)RCC_CFGR_SW_PLL;
/* Wait till PLL is used as system clock source */
while
((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)RCC_CFGR_SWS_PLL)
{
}
}
else
{
/* If HSE fails to start-up, the application will have wrong clock
configuration. User can add here some code to deal with this error */
}
}
2016-01-11 11:54 PM
This code is abstraction to your problem.
How you measure APB clock? By MCO is imposible.2016-01-12 01:24 AM
Thanks, You are rigth! I've simplified the code. I measure the PWM period of TIM3, and I see the same period with:
RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE1_DIV1;
orRCC->CFGR |= (uint32_t)RCC_CFGR_PPRE1_DIV2;
but I see double period withRCC->CFGR |= (uint32_t)RCC_CFGR_PPRE1_DIV4;
quadruple withRCC->CFGR |= (uint32_t)RCC_CFGR_PPRE1_DIV8;
2016-01-12 02:04 AM
Look to RM on picture with RCC structure.
If APB presc > 1 then TIM clk is multiply by 2.2016-01-12 02:32 AM
Here below the picture from DM00058181 pg 18:
as you said ''if (APB1 presc. = 1) x1 else x2. but this is in contrast with what I see:APB1 presc = 1 or APB1 presc = 2 , TIM3_CLK is the same!if APB1 presc = 4, TIM3_CLK double2016-01-12 02:49 AM
Consider AHB clk = 16Mhz
APB2_div = 1 -> TIM CLK = 16MHz APB2_div = 2 -> TIM CLK = 16MHz APB2_div = 4 -> TIM CLK = 8MHz APB2_div = 8 -> TIM CLK = 4MHz.2016-01-12 04:21 AM
Thanks dembek, now it's clear!
Consider AHB clk = 16MhzAPB1_div = 1 -> TIM CLK = (AHB/1)x1 = 16MHzAPB1_div = 2 -> TIM CLK = (AHB/2)x2 = 16MHzAPB1_div = 4 -> TIM CLK = (AHB/4)x2 = 8MHzAPB1_div = 8 -> TIM CLK = (AHB/8)x2 = 4MHz.