2009-01-02 4:52 AM
Analog Comparator
2011-05-17 4:34 AM
Hi,
is there an analog comparator in the stm32f103? I can't find one ... What is the best way to compare two ADC and get an interrupt? Thanks! Regards, Thorsten2011-05-17 4:34 AM
A comparator IC and a pin configured for interrupt. Or the ADC configured for measurement of those 2 values and a compare operation in the ADC interrupt.
[ This message was edited by: prx on 15-12-2009 18:22 ]2011-05-17 4:34 AM
I think the analog Watchdog is a good solution.
Is it posible to configure 4 watchdogs? In the samples I found the posibility to configure the channel or all channels and one max/min value. But I need to check 4 ADC lines with other 4 lines with different min/max values? Is this possible? If not I think an interrupt after adc conversion and check the values by code is the best solution. Regards, Thorsten2011-05-17 4:34 AM
As you seek to compare 4 channels - prx's suggestion of analog comparator IC ''jumps out.'' (many are 4 ch. in single pck)
Sometimes - temptation to ''do everything'' via MCU must be traded against the ease & much faster response of a dedicated, content-specific IC.2011-05-17 4:34 AM
thorsten.raab,
How fast do you need it to be? If it’s in the 1 to 2 microsecond range you need dedicated hardware. If you can live with 5 microseconds then ADC/DMA/ISR when all 4 are done. With a 72 MHz processor this is 4.68 microseconds for 4 conversions. Take any needed action in your ISR and restart your 8 conversions. Faster than you want? Use a timer to trigger ADC start. You can do this without using interrupts if you are able to look often enough. Use ADC/DMA in continuous mode. Use a timer to start the next conversion every 1.2 microseconds. Conversions run forever without further intervention. Look at your results any time. With 4 channels you can use the injected channels without DMA. Test carefully. It’s easy to get the channel results backwards.