cancel
Showing results for 
Search instead for 
Did you mean: 

AN2824, Optimised I2C - applicable to STM32F411 ?

Andrew Neil
Super User
Posted on May 11, 2016 at 12:26

AN2824: Application note - STM32F10xxx I2C optimized examples

''This application note applies to STM32F101xx and STM32F103xx medium, high and XL density microcontrollers, STM32F105/107xx connectivity line and STM32F100xx value line devices.''

Is it also applicable to STM32F411?

Comparing  the RM0008 (for F10x) and  RM0383 (for F411), it looks like it probably is.

See also: 

/6d281e24

 - Repeated Start Conditions

#stm32f1 #an2824 #i2c #stm32f4
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on May 23, 2016 at 16:46

Hi neil.andrew,

Besides to the reference manuals, you have to refer to the errata sheet of both products to know limitations.

The main features should be the same, I2C in STM32F411 should have less limitations than the one in STM32F1.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.