2017-10-27 8:48 AM
Hi, I have two projects. One with all the features I want to have: UART, SPI and other protocols to initialize the LCD; it was built with STM32 CUBE MX. The other project is the EEPROM Emulation modified to read some values after power on. Both are working, I want to join both to build just one project. The problem Im facing is, I tried to configure all the peripherals, the code compiles but the board doesn't do anything else but only the eeprom emulation feature. Do you know what I can be missing?
#stm32-mat #stm32f4-discovery2017-10-27 9:12 AM
>>
Do you know what I can be missing?
Most likely pin configuration or clock configuration, CubeMX tends to hide/obfuscate this stuff
Watch also for linker scripts and carving space for the EEPROM emulation out of the FLASH load region.
2018-02-23 9:14 AM
I have exactly the same problem with SensorDemo from the STM32CubeExpansion_BLE1. I try to add the UART and I2C to this demo but with no result.
In which files can I check the Pin configuration and clock configuration ?
Thanks.
2018-02-23 9:36 AM
These things are spread all over the place in examples, look in
main.h
main.c
stm32Xxxx_hal_msp.c
stm32Xxxx_hal_conf.h
C/C++ command line defines
Search (find-in-files, grep, IDE based source browsing) for HAL_XXX_MspInit() functions supporting peripherals on your board, BSP_XXX_Init() functions.
SystemClock_Config()
HAL_Init()
HAL_MspInit()
etc
When learning a new platform, third party code or porting, use Static Analysis tools like Understand(tm)