cancel
Showing results for 
Search instead for 
Did you mean: 

Add file to system workbench project

Brother Theo
Associate II
Posted on May 21, 2018 at 18:46

How do I add an external file to a system workbench project? I've done it before but the method I thought I used didn't work this time. What I did was copy the file into the SRC folder of the project, then open the project and open the new file. That didn't work. So how does one do this?

#add-external-file #system-workbench
3 REPLIES 3
John Fitter
Associate II
Posted on May 22, 2018 at 02:21

Using Eclipse I just drag the file and drop it on the project exactly where I want it.

Brother Theo
Associate II
Posted on May 22, 2018 at 07:48

I figured it out. In the project explorer at the top of the tree right click on the project name then click the refresh menu item.

Posted on May 22, 2018 at 07:28

Except this Drag-and-Drop method, the file/project import is not intuitive at all.

Find a generic Eclipse tutorial, perhaps the System Workbench has even  a useful help.