2023-12-11 02:54 PM
Hello,
I want to make a design with the ADC1283 where DVCC is powered by a 5V buck converter, and AVCC is powered off a 4.5V voltage regulator (that's powered off the buck converter). Is this possible?
I can't tell whether DVCC and AVCC are allowed to be significantly different from the datasheet.
Not sure if this is the right category in the forum or not; couldn't find one that fit.
Solved! Go to Solution.
2023-12-11 05:41 PM
> I want to make a design with the ADC1283 where DVCC is powered by a 5V buck converter, and AVCC is powered off a 4.5V voltage regulator (that's powered off the buck converter). Is this possible?
Yes, digital and analog are independent of each other. 5V and 4.5V are acceptable.
2023-12-11 05:41 PM
> I want to make a design with the ADC1283 where DVCC is powered by a 5V buck converter, and AVCC is powered off a 4.5V voltage regulator (that's powered off the buck converter). Is this possible?
Yes, digital and analog are independent of each other. 5V and 4.5V are acceptable.