cancel
Showing results for 
Search instead for 
Did you mean: 

ADC'value can't be updated after exit from stop mode

lo_529
Associate III
Posted on January 12, 2015 at 04:39

Now I'm using STM32F103RE and system will enter stop mode with a periodic RTC wakeup routine.

But sometimes when system exites from STOP MODE, the adc's value can't be updated correctly, especially when system enter STOP MODE for a long time.

OCZ, there will be a periodic RTC routine wakeup to feed WDG.

After exit from STOP mode, I re-init system clock using the example code's ''SYSCLKConfig_STOP()''. All the other peripherals work well but the ADC.

The ADC uses DMA.

So somebody can give me some advices?

#stm32f103-stop-mode-adc-dma
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0