cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4DIS-BB ethernet clock problem

peterdonchev
Senior
Posted on January 12, 2015 at 08:47

I just want to share one solution for a problem which I found on the expansion board STM32F4DIS-BB. I'm developing application which need high ethernet throughput, but faced a problem with many damaged rx frames (with bad CRC). I was sure, that this is probably a hardware problem and looked at the board schematic. W

hat

drew my

attention

was

resistor R27 (220 Ohm) on the reference clock between PHY and MCU. I

suspect

that its value was intended to be 22 Ohm, but for some reason it is 220 Ohm. After shorting it the problem

disappeared

. Not a single bad frame and the communication is now smooth and fast.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0