cancel
Showing results for 
Search instead for 
Did you mean: 

ADC self calibration

STaka.3
Associate

​Hello,

I am using STM32L471QE.

​Please tell me how to calculate CALFACT_S and use it for ADC self calibration.

I confirm that ADC1_CALFACT in CALFACT_S is 0x3A or 0x3B.

I want to know how much [CALFACT_S] affects accuracy.

Please let me know if there is a document that explains ADC self calibration in detail.

I can't understand it to read reference manual.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @STaka.3​ ,

Welcome to the STM32 Community =)

The ADC self calibration allows to cancel positive and negative offset (+/-64 LSB).

It's an offset calibration, it only corrects the offset error, and this is done automatically by the ADC when you launch a calibration.

Please double check in reference manual RM0351; this should be clear in section "18.4.8 Calibration (ADCAL, ADCALDIF, ADC_CALFACT)".

You can also review the AN2834 Application note How to get the best ADC accuracy in STM32 microcontrollers.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
STaka.3
Associate

Hello Imen DAHMEN (ST Employee)

Thank you for your answer.

I read manual RM0351.

Add Can you tell us about the following.

How to calculate CALFACT_S ?​

​VREFINT×〇〇= CALFACT_S?

The sensor output of my product is adjusted at the factory.

And store the AD value of the sensor output in the MCU.

​I am worried that the ADC self calibration cause gap of store the AD value.

​​

Shun