2018-06-28 1:18 PM
Hello everyone
i have a question, i am using 3 Ranks ADC injected mode for reading potential resistors..the problem is when ever i change one value it affects the other channel reading.example
channel 1
reading is 1.3v
channel 2
reading is 1.5v
channel 3 reading is 1.6v
changing only resistor value on channel 1 to 2.9v makes the following:
channel 1
reading is 2.9v
channel 2
reading is 1.7v
channel 3 reading is 1.7v
why when i change one value the others are affected !! or the second one affecting the third !
code is :
while (1)
{ HAL_ADCEx_InjectedStart(&hadc1); HAL_ADC_PollForConversion(&hadc1,100); u[0]=((float)HAL_ADCEx_InjectedGetValue(&hadc1,ADC_INJECTED_RANK_1))*3.0/4096.0; u[1]=((float)HAL_ADCEx_InjectedGetValue(&hadc1,ADC_INJECTED_RANK_2))*3.0/4096.0; u[2]=((float)HAL_ADCEx_InjectedGetValue(&hadc1,ADC_INJECTED_RANK_3))*3.0/4096.0; HAL_ADCEx_InjectedStop(&hadc1); sprintf(str, '%.2fv %.2fv %.2fv ', u[0], u[1], u[2]); LCD_SetPos(0,0); LCD_String(str); HAL_Delay(200); /* USER CODE END WHILE *//* USER CODE BEGIN 3 */
}
#injected-adc2018-12-18 11:30 AM
Same problem.
Who knows why and how to fix it?
2018-12-18 12:41 PM
Perhaps use a sample time setting commensurate with your ability to change the charge level on the sampling capacitor?
2018-12-19 12:40 AM
Here is the mine configuration. I changed Sample time value but no changes.
2018-12-19 12:45 AM