ADC DualMode Interl
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-29 6:51 AM
hello
I wanna use ADC Dual Mode Interl with DMA1. I use following code but it doesn't work! where is the problem?! I cannot use DMA2. Iused DMA2 for other peripheral.... &sharpinclude <stm32f4xx_gpio.h> &sharpinclude <stm32f4xx_rcc.h> &sharpinclude <stm32f4xx_tim.h> &sharpinclude ''stm32F4xx.h'' /** @addtogroup STM32F4_Discovery_Peripheral_Examples * @{ */ /** @addtogroup ADC_Interleaved_DMAmode2 * @{ */ /* Private typedef -----------------------------------------------------------*/ /* Private define ------------------------------------------------------------*/ &sharpdefine ADC_CDR_ADDRESS ((uint32_t)0x40012308) /* Private macro -------------------------------------------------------------*/ /* Private variables ---------------------------------------------------------*/ __IO uint32_t ADCDualConvertedValue[2]; ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; DMA_InitTypeDef DMA_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Private function prototypes -----------------------------------------------*/ /* Private functions ---------------------------------------------------------*/ /** * @brief Main program * @param None * @retval None */ int main(void) { /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f4xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f4xx.c file */ /******************************************************************************/ /* ADCs interface clock, pin and DMA configuration */ /******************************************************************************/ /* Enable peripheral clocks */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1 | RCC_AHB1Periph_GPIOC, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_ADC2 , ENABLE); /* Configure ADC Channel 12 pin as analog input */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOC, &GPIO_InitStructure); /* DMA1 Stream5 channel7 configuration */ DMA_InitStructure.DMA_Channel = DMA_Channel_7; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC_CDR_ADDRESS; DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCDualConvertedValue; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 2; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA1_Stream5, &DMA_InitStructure); /* DMA1_Stream5 enable */ DMA_Cmd(DMA1_Stream5, ENABLE); /******************************************************************************/ /* ADCs configuration: triple interleaved with 5cycles delay to reach 6Msps */ /******************************************************************************/ /* ADC Common configuration *************************************************/ ADC_CommonInitStructure.ADC_Mode = ADC_DualMode_Interl; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_2; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC1 regular channel 12 configuration ************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC1, &ADC_InitStructure); ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 1, ADC_SampleTime_3Cycles); /* Enable ADC1 DMA */ ADC_DMACmd(ADC1, ENABLE); /* ADC2 regular channel 12 configuration ************************************/ ADC_Init(ADC2, &ADC_InitStructure); /* ADC2 regular channel12 configuration */ ADC_RegularChannelConfig(ADC2, ADC_Channel_12, 1, ADC_SampleTime_3Cycles); /* Enable DMA request after last transfer (multi-ADC mode) ******************/ ADC_MultiModeDMARequestAfterLastTransferCmd(ENABLE); /* Enable ADC1 **************************************************************/ ADC_Cmd(ADC1, ENABLE); /* Enable ADC2 **************************************************************/ ADC_Cmd(ADC2, ENABLE); /* Start ADC1 Software Conversion */ ADC_SoftwareStartConv(ADC1); while (1) { } } #rtfm- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-01-01 6:46 AM
baird.hal, many thanks for your answer. I used DMA2 for two peripheral and it worked. I didn't test DMA2 for two peripheral before and I didn't think that may work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-01-01 6:49 AM
clive, your right. I made mistake between DAC and ADC. the stream and channel I said in my last post was for DAC!! I use DMA2. it do well...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-29 7:12 AM
I believe the peripheral assignments to DMA/Channel/Stream are fixed as defined in section 4.3.3 of the reference manual. Use DMA2 for more than one peripheral.
Cheers, Hal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-29 12:28 PM
Look you can't just invent random connectivity in your head. The DMA channels/streams have very specific connections. DMA2 has EIGHT independent streams, TWO available to ADC1. DMA1 has ZERO available to ADC1, and thus will NEVER work.
http://www.st.com/web/en/resource/technical/document/reference_manual/DM00031020.pdf
Up vote any posts that you find helpful, it shows what's working..