Problem with ADC Dualmode with 12 bit and DMA
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-02-23 7:58 AM
Posted on February 23, 2017 at 16:58
Hello, I am using the stm32f334 and try to use both adc in dual mode with 12 bit and one dma channel. With 8 bit halfword everything works fine. But when i use 12bit and DMA set to WORD array and HAL_ADC_GETVALUE (assume it is the right value) does not match anymore. In the dma array is just really low values. Have anyone an idea what could be the problem? Thank a lot....
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0